The Add-On Instruction Definition exceeds the maximum allowed Input and Output Parameters and Local Tags

The Add-On Instruction Definition exceeds the maximum allowed Input and Output Parameters and Local Tags

This error appears when your changes to an Add-On Instruction definition cannot be saved. You have defined too many input and output parameters and local tags for the Add-On Instruction.
Remove input and output parameters or local tags until their combined number does not exceed the 512 maximum allowed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal