- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Failed to change instruction's Class to Safety
Instruction contains data types invalid for use in Safety.
The
Logix Designer
application prevents the modification of a User Defined or Add-On Defined type that would cause an invalid data type for User Defined or Add-On Defined types that are referenced directly or indirectly by a Safety
tag. (This includes nested structures.) The
invalid
data types are:- REAL - Only invalid on GuardLogix(L6S) and Compact GuardLogix(L4S) controllers
- LINT
- ALARM-ANALOG
- ALARM DIGITAL
ST Prescan routine is invalid for Safety.
Safety only supports RLL.
Safety add-on instructions don't support Postscan routines.
Postscan routines are not supported in Safety add-on instructions. Safety only supports RLL.
FBD EnableInFalse routine is invalid for Safety.
FBD EnableInFalse routines are not supported in Safety add-on instructions. Safety only supports RLL.
For more information, see
Safety Add-On Instruction class change
.Provide Feedback