- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add-On Instruction Definition Editor Dialog - Help Tab Overview
This tab displays auto-generated Help text for the Instruction and lets you add extended description text. This content reflects updates as Parameters or other attributes are changed in the definition.
Attributes
Extended Description Text
Enter extended description text for the Instruction help. Carriage returns and tabs are preserved. The content entered here is added to the Instruction Help for this instruction.
Instruction Help Preview
See a preview of the instruction help that is available if you press the [F1] key or click the Help button from the instruction browser (read-only).
Logic
Click to open the Logic routine. This Logic button is not visible if the Add-On Instruction is source-protected.
Data Type Size
Displays the size of the Add-On Instruction data type – this does include the size of any Local Tags (even though Local Tags are not visible when an instance tag of this data type is expanded in the Tag Editor or Data Monitor), but it does not include logic size. The size is automatically updated when you apply the instruction, not as you create the Parameters and Local Tags.
Copy all default values of parameters and local tags whose values were modified to all tags of this instruction type
Copies all the default values of the parameters/local tags, or members' default values, that you have changed, to all instance tags of this instruction type.
OK
Click this button to accept your edits and close the Add-On Instruction Definition Editor dialog box.
Cancel
Click this button to cancel your edits and close the Add-On Instruction Definition Editor dialog box.
Help
Click this button for help on this tab.
Provide Feedback