- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Instruction Name Collision dialog box - Property Compare tab
Use this dialog box to compare the differences between new and existing Add-On Instructions.
- An attribute list displays the existing Add-On Instruction to the one being copied and pasted for easy comparison. The attribute list is read-only.
- For attributes that are different, the name of the attribute is in bold type and the entire line is highlighted in pale yellow.
Overwrite
Select this button to set
Overwrite
as the operation for this instruction and close the Instruction Name Collision
dialog box.Cancel
Close the
Instruction Name Collision
dialog box without overwriting the Add-On Instruction.Provide Feedback