- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Advanced Project Documentation Configuration dialog box overview
Use the Advanced Project Documentation Configuration dialog box to configure the language localization that is downloaded to the controller.
Use the
Download Controller Description Language
parameter to switch the currently used documentation language, which changes the language used to display all project documentation.You can select languages that do not currently have content. The result is blank project documentation (if no default language is chosen) is displayed for the project. The description of the controller is the only documentation downloaded to the controller. Only one translation of the description may exist in the controller at a time.
Provide Feedback