- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Dependent vertical load attributes
The
Vertical Load Control
setting has changed, which affects the values of other attributes. The current list of affected attributes includes:- Brake Prove Ramp Time
- Brake Slip Tolerance
- Brake Test Torque
- Coasting Time Limit
- Connection Loss Stopping Action
- Mechanical Brake Release Delay
- Mechanical Brake Engage Delay
- Proving Configuration
- Safe Torque Action Source
- Safe Torque Off Action
- Stopping Action
- Torque Prove Current
- Zero Speed
Provide Feedback