- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Homing page
Use the settings on the
Homing
page to:- Select a homing mode.
- Select the home position of the motor.
- Specify the offset of the axis from the home position.
- Select the homing sequence.
- Select if the limit switch is open or closed.
- Configure direction, speed, torque level and return speed for an active homing sequence.
- Access theHookup Testsdialog box to determine motor and feedback polarity.
TIP:
To open the Homing page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickHoming.
These are the Homing page parameters.
Parameter | Description |
---|---|
Mode | Determines if homing actively moves the axis to generate the homing event or if some external agent moves the axis to generate the homing event. Available options:
|
Position | Specifies the home location of the motor in user defined position units. |
Offset | Specifies the amount the axis is offset from the home position in user defined position units. |
Sequence | Determines the motion sequencing that triggers the desired homing events. Available options:
|
Torque Level | Specifies the torque level as a percentage of continuous torque that the motor uses to return to the home position. |
Limit Switch | Determines if the limit switch is normally Open or Closed . This parameter is available when Sequence is set to Switch or Switch-Maker . |
Active Homing Sequence Group | These parameters are available when Mode is set to Active and Sequence is not set to Immediate . |
Direction | Determines the direction the motor takes to reach the home position. Available options:
|
Speed | Enter a value, in user defined position units, for the speed the motor uses to reach the home position. |
Torque Level | Specifies the torque level as a percentage of continuous torque that the motor uses to return to the home position. |
Return Speed | Enter a value, user defined position units, for the speed the motor uses to return to the home position. |
Test Marker | Opens the Hookup Tests dialog box to determine motor and feedback polarity.This button appears dimmed in offline mode and when online in Servo On mode. |
Provide Feedback