- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Editing Controller Properties
Use the
Controller Properties
dialog box to configure the controller.
ATTENTION:
Changing from a safety controller to a standard controller is not an option if the project contains safety Add-On Instructions. The safety Add-On Instructions must either be converted to standard Add-On Instructions or deleted from the project. Then the conversion is allowed.
To edit controller properties:
- On theOnlinetoolbar, select theController Propertiesicon.
- Select theGeneraltab and configure the controller name and description, as well as its physical description, using these parameters:
- Vendor
- Type
- Revision
- Name
- Description
- Chassis Type
- SlotTIP:
- Select theChange Controllerbutton to change to a different controller type or revision.
- Select theChangeIP Modebutton to change the Ethernet/IP mode of the Ethernet port on a controller that supports dual configurable Ethernet ports, for example theCompactLogix5380.
- Select theMajor Faultstab to view any major fault information and clear the faults as appropriate.
- Select theMinor Faultstab to view any minor fault information and clear the faults as appropriate.
- Select theDate/Timetab to configure the controller’s wall clock time and enable time synchronization.
- Select theAdvancedtab to configure advanced controller properties such as Controller Fault Handler program, Power-Up Handler program, system task overhead, security, and controller serial number.
- Select theCapacitytab to view the size of the source code of the application.
- Select theSFC Executiontab to configure sequential function chart execution.
- Select theProjecttab to view information about the project file (that is, not about the controller itself).
- If online and connected, select theNonvolatile Memorytab (where available) to configure nonvolatile memory operations.
- Select theSafetytab to view and edit safety properties for the Safety controller, such as Safety application's Lock/Unlock status, Safety Network Number, Safety Signature, and Safety Level.TIP:Additional tabs may appear depending on the type of controller and its configuration.
- Select theOKbutton to accept the configuration and close theController Propertiesdialog box.
Provide Feedback