Enable PlantPAx settings

Enable PlantPAx settings

Enable settings such as tasking model and instruction usage on PlantPAx controller projects to:
  • Use a predefined set of tasks with simplified configuration. Enabling tasking model creates projects that conform to
    Rockwell Automation®
    recommendations for the PlantPAx controller.
  • View which PlantPAx and process instructions are used in which tasks. This view provides a way to see the overall process execution load on a project for each task.
    TIP:
    The tasking model option is enabled by default unless the existing project was converted to a PlantPAx controller from another controller type.
To enable PlantPAx settings
  1. Create a project with a PlantPAx controller.
    TIP:
    When working with existing projects, the project must use a process controller to access PlantPAx
    controller options.
  2. Open the
    Controller Properties
    dialog box and select the
    PlantPAx
    tab.
  3. Select
    Use PlantPAx Tasking Model
    to use a predefined set of tasks with default configuration and editing restrictions.
  4. Select
    Instruction Usage
    to view which PlantPAx and process instructions are used in which task.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal