Tracked Components dialog box

Tracked Components dialog box

The
Tracked Components
dialog box lists tracked components and displays one overall tracked value to indicate their current state. When a component changes, the compiled value updates to indicate a change occurred.
Use the
Show
menu to filter the tracked components based on component type. Use the
Search
box to find a specific component. The number of tracked components appears at the lower left in the dialog box.
TIP:
The
Tracked State
value and the list of tracked components are static as long as the dialog box is open and will not reflect changes from other workstations. If a user on another workstation makes an update, if changes are not showing, close and re-open the
Tracked Components
dialog box to see the changes.
TIP: To open the Tracked Components dialog:
  1. On the
    Online
    toolbar, click the
    Controller Properties
    icon.
  2. On the
    Controller Properties
    dialog box, click the
    Security
    tab.
  3. Click
    View Components
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal