Equipment Phase Properties - General tab fields

Equipment Phase Properties - General tab fields

Use the
General
tab of the
Equipment Phase
Properties
dialog to modify the name and description of the
Equipment Phase
. These options are available on the
General
tab.
L5K_EquipmentPhaseProperties_GeneralTab
Name
Purpose
1
Name
The sequence name, which must follow the IEC-61131 Name Standard. The application ignores invalid characters.
2
Description
Enter the optional description for this <EP>. Language switching is provided for this control.
3
Schedule in
Displays the task that runs the
Equipment Phase
program.
OK
Select to accept edits. If all attributes are valid, the modified attributes save for the current equipment phase and the dialog closes.
OK
and
Apply
are not available if the dialog box contains invalid data.
Cancel
Select to cancel edits and close the
Equipment Phase Properties
dialog.
Apply
Select to apply edits and continue editing in the
Equipment Phase Properties
dialog. Applying edits runs the same validation as selecting
OK
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal