- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Import/Paste Configuration dialog - Routines tab
Use this dialog to view routine definitions. All settings in this dialog are read-only and cannot be changed.
TIP:
To open the Import/Paste Configuration dialog - Routines tab:
- SelectFile > Import Component > <component>.
- Select a component for import and selectOpen.
- On theImport Contentpane, selectRoutines.
The dialog lists information for imported routines from a program,
Equipment Phase
, or Add-On Instruction, and for the Diagram routine from an imported Equipment Sequence
. When you select Routines
in the Import Content
pane, the routine definitions grid view displays in the Details pane. The routine definitions grid contains the union of all the routines that appear in both the import content and the project, and shows the disposition of each. For example, if a routine exists in the program in the project, but does not exist in the program being imported, the operation for that routine is set to Delete
.The
Operation
setting for these routines is based on the Operation chosen for the component being imported.The routines item does not display if:
- The Add-On Instruction of which it is a part is protected and not viewable.
- Collides with an Add-On Instruction in the project that is protected and not viewable.
Provide Feedback