Add a description to an Equipment Sequence diagram

Add a description to an Equipment Sequence diagram

Add a description to an
Equipment Sequence
diagram using the
Routine Properties
dialog box.
Before you begin:
  • Go offline with the controller.
  • Right-click on the
    Equipment Sequence
    diagram in the
    Controller Organizer
    or
    Logical Organizer
    and then select
    Properties.
To add a description to an
Equipment Sequence
diagram:
  1. In the
    Routine Properties > General tab
    , enter a description for this
    Equipment Sequence
    diagram.
  2. Select
    OK
    to save the
    Equipment Sequence
    diagram description, or select
    Cancel
    to discard all changes and close the dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal