PIDE Autotune Dialog Box Overview

PIDE Autotune Dialog Box Overview

The Enhanced Proportional Integral Derivative (PIDE) instruction provides enhanced capabilities over the standard PID instruction for control of process variables (PV) such as flow, pressure, temperature, or level. The Logix Designer application PIDE autotuner provides an open-loop autotuner built into the PIDE instruction. You can autotune from PanelView terminals or any other operator interface devices, as well as the Logix Designer application. The PIDE block has an Autotune Tag (type PIDE_AUTOTUNE) that you specify for those PIDE blocks that you want to autotune.
Use the
PIDE Autotune
dialog bo to autotune your PIDE block, select or configure the gains, and then load the gains into the controller.
The following table describes the parameters available on the
PIDE Autotune
tab.
Parameter
Description
Start
Click this button to begin the autotune process. Note that the PIDE loop must be in Manual in order for the autotuning to proceed.
Abort
Click this button to abort the autotune process.
Execution State
The current state of the autotune process. Displays either:
  • Ready
  • In Progress
  • Complete
  • Aborted
Autotune Status
Displays detailed fault status information, if any.
Autotune Gains Buttons
Select the appropriate combination of check boxes, based on the gains you want to download to the controller.
If you select
Slow
,
Medium
, or
Fast Response
, the
ResponseSpeed
parameter is adjusted accordingly.
If you choose
Current
, then the
Proportional
,
Integral
, and
Derivative
fields are enabled, and you can adjust them accordingly.
Slow Response, Proportional
Displays the value of the
PgainTunedSlow
autotune parameter.
Slow Response, Integral
Displays the value of the
IgainTunedSlow
autotune parameter.
Slow Response, Derivative
Displays the value of the
DgainTunedSlow
autotune parameter.
Medium Response, Proportional
Displays the value of the
PgainTunedSlow
autotune parameter.
Medium Response, Integral
Displays the value of the
IgainTunedMed
autotune parameter.
Medium Response, Integral
Displays the value of the
IgainTunedMed
autotune parameter.
Medium Response, Derivative
Displays the value of the
DgainTunedMed
autotune parameter.
Fast Response, Proportional
Displays the value of the
PgainTunedFast
autotune parameter.
Fast Response, Integral
Displays the value of the
IgainTunedFast
autotune parameter.
Fast Response, Derivative
Displays the value of the
DgainTunedFast
autotune parameter.
Current, Proportional
Displays the value of the
PGain PIDE
parameter.
Current, Integral
Displays the value of the
IGain PIDE
parameter.
Current, Derivative
Displays the value of the
DGain PIDE
parameter.
Set Gains in PIDE
Click this button to set the PIDE current gains with the selected tuned gains.
Time Constant
Displays the value of the
TimeConstant
autotune parameter. This shows the first order lag time constant used by the process model estimated by the autotuning algorithm. This value, along with the
Deadtime
and
Gain
, allows you to estimate the accuracy of the tuning constants derived by the autotuner.
Deadtime
Displays the value of the
DeadTime
autotune parameter. This shows the deadtime used by the process model estimated by the autotuning algorithm. This value, along with the
Time Constant
and
Gain
, allows you to estimate the accuracy of the tuning constants derived by the autotuner.
Gain
Displays the value of the
Gain
autotune parameter. This shows the process gain used by the process model estimated by the autotuning algorithm. This value, along with the
Time Constant
and
Deadtime
, allows you to estimate the accuracy of the tuning constants derived by the autotuner.
Close
Click this button to close the
PIDE Autotune
dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal