- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Drive
Data exchange is not supported for these drives.
Drives
Catalog Number or Product Family | RDF support | AML support |
---|---|---|
1305-ACDrive-CN1 | No | No |
1305-ACDrive-EN1 | No | No |
1336E-IMPACTDrive-CN1 | No | No |
1336E-IMPACTDrive-EN1 | No | No |
1336F-PLUSIIDrive-CN1 | No | No |
1336F-PLUSIIDrive-EN1 | No | No |
1336R-REGENBrake-CN1 | No | No |
1336R-REGENBrake-EN1 | No | No |
1336S-PLUSDriveLG-CN1 | No | No |
1336S-PLUSDriveLG-EN1 | No | No |
1336S-PLUSDriveSM-CN1 | No | No |
1336S-PLUSDriveSM-EN1 | No | No |
1336T | No | No |
1336T-FORCEDriveCNA-CN1 | No | No |
1336T-FORCEDriveCNA-EN1 | No | No |
1336T-FORCEDrivePLC-CN1 | No | No |
1336T-FORCEDrivePLC-EN1 | No | No |
1336T-FORCEDriveStd-CN1 | No | No |
1336T-FORCEDriveStd-EN1 | No | No |
1394C-SJT05-D | No | No |
1394C-SJT10-D | No | No |
1394C-SJT22-D | No | No |
1395 | No | No |
1397DigitalDCDrive-CN1 | No | No |
1397DigitalDCDrive-EN1 | No | No |
150-SMC Flex-C | No | No |
150-SMC Flex-E | No | No |
150-SMC Flex-ER | No | No |
150-SMC Flex-Q | No | No |
150-SMCDialogPlus--CN1 | No | No |
150-SMCDialogPlus--EN1 | No | No |
2098-DSD* | No | No |
2099-BM* | No | No |
2364F-RGU* | No | No |
8720MC* | No | No |
Drives AOP Infrastructure | No | No |
FLEX-MODULE | No | No |
Generic SERCOS Drive | No | No |
GV3000 | No | No |
Multi-Drive-25-COMM-E2P | No | No |
Rockwell Automation UDC AOP Infrastructure | No | No |
SMC-50* | No | No |
WebPak 3000 | No | No |
* All devices of type |
Provide Feedback