PID Configuration Dialog Box - Scaling Tab Overview
Use this tab to set up the PID scaling and limits.
Parameters
Unscaled Max
The maximum value for the unscaled Process Variable (PV).
Unscaled Min
The minimum value for the unscaled Process Variable (PV).
Engineering Unit Max
The maximum engineering unit for the Process Variable (PV).
Engineering Unit Min
The minimum engineering unit for the Process Variable (PV).
Max
The maximum value for the Control Variable (CV).
Min
The minimum value for the Control Variable (CV).
Max
The maximum value for the Tieback value.
Min
The minimum value for the Tieback value.
PID Initialized
Indicates whether the PID value has been initialized.
Provide Feedback