- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Change Add-On-Instruction preferences
Use the
Print Options
dialog box to select the Add-On Instruction information you want to include in your report.To change Add-On Instruction preferences:
- From the main menu, selectFile>Print Options.
- From thePrintdialog box, selectPrint Options.
- Select the Add-On-Instructions category and select or clear the following:Name, Revision Information, and Description.Indicates that the instruction's name, revision identifier, revision note, and description print as part of the report.Instruction help.Prints the generated instruction help in the report.Change History.Includes change history listing showing when the Add-On Instruction was created and last edited.Signature and Signature History.Prints the signature id and timestamp as well as the signature history (including the user, id, timestamp, and description).Cross Reference.Includes a cross reference listing showing where actual instances of this instruction are within the project.Parameter Listing.Determines whether parameter information (for example, type, format, description) are included in the listing.Note that some of this information is a superset of the parameter information printed as part of the Instruction Help, including all of the configuration attributes for each parameter. Tag Listing options are also followed when they apply (such as cross reference, special properties, expand data types, and pass through descriptions).Local Tag Listing.Includes information similar to the Tag Listing report for the local tags used within the Add-On-Instructions definition. Tag Listing options are also followed when they apply.Routine Listing.Determines whether the Add-On-Instruction logic should be printed with the rest of the report. If selected, all logic, including the scan mode routines, are printed in the report.
- SelectOK.
Provide Feedback