Change General report preferences
Use the
Print Options
dialog box to select the information you want to include in all of the reports.To change general report preferences:
- From the main menu, selectFile>Print Options.
- From thePrintdialog box, selectPrint Options.
- Select theGeneralcategory, and select or clear the following:
- Include footer text.Enter up to 128 characters of text to be printed at the bottom of each page.
- Print Grid.Print grid lines in your sequential function chart and function block diagram routines.
- SelectOK.
Provide Feedback