Configure Page Setup

Configure Page Setup

Use this dialog to specify the margins, orientation, and paper used when a report is printed.
To configure the page setup of your reports.
  1. From the main menu, select
    File > Page Setup
    .
  2. From the
    Generate Report
    dialog box, click
    Page Setup
    .
  3. In the
    Margins
    section, enter the values you wish to use for your left, right, top, and bottom margins.
  4. In the
    Orientation
    section, to specify your page orientation, select either Portrait or Landscape.
    Note that for SFC and FBD routines, the Sheet Layout orientation overrides this value.
  5. In the
    Paper
    section, select the size and source for the paper.
  6. (optional) To select a different printer, click
    Printer
    .
    The
    Printer
    button is only available for the
    Logix Designer
    application that is run on an operating system earlier than
    Windows Vista
    . To access the printer selection option in
    Windows Vista
    and later operating systems, press Ctrl + P to open the
    Print
    dialog box.
  7. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal