Generate multiple reports

Generate multiple reports

You can generate multiple reports for the components in the
Controller Organizer
.
To generate reports:
  1. Select
    File > Generate Report
    to open the
    Generate Report
    dialog box.
  2. Under
    Component Selection
    , select the components in your project for which you are generating reports. Not all components are selected by default. To determine which components are selected, refer to the following icons:
    Parent_AllChildren - The parent and all of its children are selected
    NoParent_SomeChildren - The parent is not selected, but some (not all) of its children are selected
    Child - A child is selected (you can select a child without necessarily selecting its parent)
    TIP:
    The Child icon is also displayed when you select the Add-On Instructions component folder without selecting any of its children. When this icon is displayed, Add-On Instruction Signature Listing, which includes the ID and timestamp for all sealed Add-On Instructions, is the only report selection option available for Add-On Instructions.
  3. Under
    Report Selection
    , select whether you want to print a table of contents for your reports, and then select the reports you want to generate. By default, when the Tag Listing, Data Type Listing, and Module Properties Listing reports are displayed, they are selected.
    The reports that appear depend on the components you select. For example, the Controller Organizer Listing and Controller Properties Listing reports appear only if you select the controller folder under
    Component Selection
    .
  4. Select
    Print
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal