Argument List dialog box - GSV/SSV instruction

Argument List dialog box - GSV/SSV instruction

From this dialog box, set the arguments for the GSV or SSV instruction. The following table describes the Argument List parameters.
Parameter
Description
Class Name
The name of the object.
Instance Name
The name of the specific object, when the object requires a name. This field is enabled when the class name requires you to identify a specific instance of the object. The choices available for this field are determined by the class of the object.
If class is
Module
, and the instruction is inside an Add-On Instruction, then clicking this field displays a list of InOut parameters with MODULE data type. Outside of an Add-on Instruction, clicking this field displays the module browser so you can select a MODULE parameter or a module.
Attribute Name
The attribute of the object. The data type depends upon the attribute you choose. Attribute choices available are determined by the class of the object.
Dest (GSV only)
The destination for the attribute data. The choices available for this field are determined by the class of the object.
Source (SSV only)
The source for the attribute data. The choices available for this field are determined by the class of the object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal