- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Edit external routine properties
To edit external routine properties:
- In the Controller Organizer, right click the active routine and chooseProperties.
- InName, type a name for the external routine.
- (optional) InDescription, enter a description of the routine.
- Click theConfigurationtab to configure the rest of the properties of this routine.
- ClickOKto close theRoutine Propertiesdialog box.
Provide Feedback