- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
New Trend Dialog Box Overview
Use this dialog to create a new trend.
Parameters
Parameter | Usage |
Name | Enter the name of the trend, with a maximum length of 40 characters. This name must be IEC-1131 compliant. The software ignores any invalid characters, or any characters you enter beyond the maximum length of 40 characters. |
Description | Enter a description of the trend with a maximum length of 128 characters. |
Sample Period | Enter the sampling rate of trending in the controller. Valid values range from 1 millisecond to 30 minutes. |
OK | Select this button to accept the information you have entered and create the new trend. |
Cancel | Select this button to cancel the creation of the new trend. |
Provide Feedback