View Designer

View Designer

The following diagram shows how
View Designer
works with the
Studio 5000
suite to create a control and visualization system to monitor and control the manufacturing process.
A diagram showing how View Designer works with the Studio 5000 suite.
Item
Name
Description
1
View Designer
Build the projects that are downloaded to an HMI device.
2
Tag Browser
Search for and select tags within a
Logix Designer
project file to bind the tags to the properties of graphic elements and screens in the
View Designer
project.
3
Logix Designer
Develop control logic for an industrial automation system.
4
ACD file
The Automation Control Database (ACD) file that is the
Logix Designer
project file containing the logic or code, including tags and data types, that runs within a controller.
View Designer
uses the
Tag Browser
to read data from the ACD file.
5
HMI project
The user-defined screens, controller references, information about the target HMI device, and so forth. Projects are stored in files with a .vpd extension.
6
View Designer
Download Runtime Application Wizard
Transfer the HMI project to the HMI device.
7
HMI device
The Human Machine Interface (HMI) device, such as a PanelView 5000 device, that runs the HMI project. At runtime, the HMI device communicates directly with the controllers.
8
VPDR file
Save a Runtime Application VPDR file from
View Designer
.
9
Load from media
Load a Runtime Application VPDR file from removable media such as an SD Card or USB storage device to the HMI device.
10
Controller
A controller with the ACD file and tags used in the
View Designer
project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.