- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
CommonControls
The
CommonControls
category in the Toolbox
contains the most common graphic elements added to a screen. The graphic elements in CommonControls
are organized into categories: - Button
- DateTimeDisplay
- Image
- NumericDisplay
- NumericInput
- TextDisplay
- TextInput
- Slider Horizontal
- Slider Vertical
Provide Feedback