- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Project Events Status Indicator
The Project Events Status Indicator is predefined to open an error list displaying project event errors. This graphic element appears in the
System
category of the Toolbox
. Use the Project Events Status Indicator to:
- See a visual indicator when there is an issue with project events.
- Display an error list showing project event errors.
Common Properties
Common properties exist for all graphic elements.
Property | Category | Purpose | Accepted Values |
Access | Security | Specifies if all users have access to the control element, or if access is inherited from the screen. |
|
Angle | Position and Size | Specifies the rotation angle. Enter 180 to display the graphic element upside down. If you enter a value larger than 360, the portion of numeric value that is over 360 becomes the value. For example, enter 380 to see a value of 20. If you enter a value less than 0, the negative value is subtracted from 360. For example, enter -30 to see a value of 330. |
|
Enabled | Appearance | Specifies if the graphic element is available on the HMI device and if the graphic element accepts touch and key input. |
|
Height | Position and Size | Specifies the height in pixels. | Any positive numeric value |
Opacity | Appearance | Specifies the transparency of the graphic element. | 0 (fully transparent) - 100 (fully opaque) |
Visible | Appearance | Specifies if the graphic element is visible on the HMI device. |
|
Width | Position and Size | Specifies the width in pixels. | Any positive number |
X | Position and Size | Specifies the horizontal coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the X property value does not change. | Any positive number |
Y | Position and Size | Specifies the vertical coordinate, in pixels, from the upper left corner of screen to the upper left corner of a graphic element or group with no rotation. If the graphic element or group is rotated, the Y property value does not change. | Any positive number |
Provide Feedback