- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Add a Slider
Add a Slider graphic element to incrementally adjust numeric values for a tag within a configured range on an HMI device.
To add a Slider:
- In theToolbox, expand theCommonControlscategory.
- Drag a horizontal or vertical Slider graphic element onto the screen, popup, or Add-On-Graphic. Double-click a graphic element in theToolboxto add it to the center of the screen. If a Slider is already selected on the screen, the new Slider is placed on top of the selected graphic element.TIP:Tips:
- If the outline of an empty Add-On Graphic appears on the screen, the definition of the Add-On Graphic is empty. Add graphic elements to the Add-On Graphic by changing the definition of the Add-On Graphic. All instances of the Add-On Graphic then update to display the contents of the Add-On Graphic.
- Add a graphic element used in a different project by copying and pasting the graphic element between the projects.
- Use the search feature to search for a name or type of graphic element for the Toolbox.
- The name of each graphic element ends with a number that increments by one when adding an instance of that element. For example, TextDisplay_002 indicates a second instance of the Text Display graphic element on the screen.
- In thePropertieswindow, select thePropertiestab.
- Expand the categories and configure the Slider properties:
- General -Specify the Slider control values, and when the Slider control updates the values.
- Appearance- Specify appearance properties for the slider.
- Thumb- Specify border and fill color, style, thickness, shape, and visibility properties for the Slider thumb.
- Track- Specify border and fill color, style, thickness, and visibility properties for the Slider track.TIP:Bind a Slider property value to another property or data item to change the slider property dynamically at runtime.
IMPORTANT:
The Slider Vertical and Slider Horizontal graphic elements do not support LINT data types. An error occurs when using a LINT data type with a value property in a Slider.
Provide Feedback