Change the text in a graphic element

Change the text in a graphic element

Change the text in any graphic element that displays text. For example, change the text on a button in the project.
To change the text in a graphic element:
  • On the screen, double-click the graphic element to highlight the text and type the new text.
    TIP:
    Tips:
    • Resizing the width of a graphic element that displays text wraps the text as necessary.
    • Resizing the height of a graphic element that displays text does not resize the text to fit. Resize the height of the graphic element to display the text.
    • As an alternative, on the
      Properties
      tab, type the text in the
      Text
      property box for the graphic element.
    • To resize the text within a graphic element while resizing the graphic element, hold
      Ctrl
      while dragging a sizing handle.
    • Resizing an instance of an Add-On Graphic scales the text of any graphic element contained in the definition of the Add-On Graphic.
    • View Designer
      supports Unicode characters that appear in the Arial Unicode MS font. When inserting text that contains Unicode characters in a graphic element, select
      Arial Unicode MS
      in the
      FontName
      property of the graphic element. Supported Unicode characters appear on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.