- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Group graphic elements
Combine graphic elements and Add-On Graphics into a group to work with them as a single element. Work with the elements as a group or manipulate the individual elements within the group. Groups can contain groups.
To group graphic elements:
View Designer
names each group. Rename groups using the Name
box in the Properties
tab. The Properties
tab displays the properties to change for the group. View and work with the contents of a group in the Graphic Explorer
.- On the screen or in theGraphic Explorer, select the graphic elements and Add-On Graphics to include in the group.
- Right-click one of the selected elements and selectGroup.
TIP:
Alternate methods of grouping:
- On theDrawingtoolbar, selectGroup.
- On theStandardmenu, selectArrange > Group.
- PressCtrl+G.
Provide Feedback