- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Select a graphic element on a screen
Select single or multiple graphic elements on a screen to perform actions or display properties.
To select a graphic element on a screen
- Select individual or multiple graphic elements:
- Single graphic element.Select the graphic element.
- Multiple graphic elements.Select the screen canvas above the graphic elements and drag diagonally to create a selection border around the graphic elements. When all the graphic elements are inside the border, release the mouse button. Sizing handles on all of the selected graphic elements replace the border.
- Additional graphic elements outside of selection.To select graphic elements that are outside of the border, press and holdCtrlwhile selecting each additional graphic element, or holdCtrlwhile dragging to select additional graphic elements.
- All graphic elements on a screen.PressCtrl+A.TIP:Tips:
- To deselect all selected graphic elements, select the screen.
- If a screen contains a lot of content or overlapping graphic elements, use theGraphic Explorerto select a graphic element from a list of the graphic elements contained on the screen.
Provide Feedback