- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Add a PDF document to an Add-On Graphic
Add a PDF document to an Add-On Graphic to have the Add-On Graphic display the PDF document on the HMI device.
Prerequisites
- (optional) Create bookmarks for the PDF document prior to adding the document to the project.
To add a PDF document to an Add-On Graphic
- Open the definition of the Add-On Graphic.
- In theProject Explorer, expand theAssets > Documentsfolder.
- Drag the PDF document to the definition of the Add-On Graphic. A PDF graphic element appears in the definition of the Add-On Graphic and shows the PDF document.Tips:
- TheSelect PDF Viewerdialog does not open when adding a PDF document to an Add-On Graphic.View Designerdoes not support adding a PDF Viewer Add-On Graphic to anther Add-On Graphic.
- Dragging the PDF graphic element from theSystemcategory of theToolboxopens theSelect PDF Viewerdialog box.
Provide Feedback