Change the definition of a PDF Viewer Add-On Graphic

Change the definition of a PDF Viewer Add-On Graphic

Add, remove, rearrange, and configure content in the definition of a PDF Viewer Add-On Graphic. Do this to modify a predefined PDF Viewer Add-On Graphic instead of using a PDF graphic element and adding required functionality to that graphic element.
To change the definition of a PDF Viewer Add-On Graphic
  1. Double-click the definition of the PDF Viewer Add-On Graphic in the
    Project Explorer
    . The definition of the Add-On Graphic opens.
  2. Change the PDF Viewer Add-On Graphic:
    • Add content.
      Add graphic elements to the PDF Viewer Add-On Graphic.
    • Remove content.
      Select and delete graphic elements from the PDF Viewer Add-On Graphic to remove buttons from the Add-On Graphic.
    • Rearrange content.
      Drag to resize or change the order of content in the PDF Viewer Add-On Graphic. Do this to change the order and size of buttons in the Add-On Graphic.
    • Configure content.
      Change attributes of content in the Add-On Graphic by changing the property values, binding, animations, and events for a graphic element within the open definition of the Add-On Graphic.
  3. To close and save the definition of the PDF Viewer Add-On Graphic, on the tab of the open Add-On Graphic, select
    Close
    Close button in Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.