- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Add an event command to delete a certificate
Delete a certificate to no longer store the certificate on the HMI device.
Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when
- Key release.Occurs when releasing the specified key.
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Certificatecommand category and selectDelete Certificate. - In theFingerprintbox, type the fingerprint of the certificate or create a binding to a string containing the fingerprint of the certificate.
Provide Feedback