- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Add an event command to import a certificate
Import a certificate to allow encrypted communication between the web browser on the HMI device and a remote server.
TIP:
When creating a self-signed certificate, verify that the
Subject Alternative Name
property of the certificate contains the IP address of the device or server that you are connecting to.Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when
- Key release.Occurs when releasing the specified key.
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Certificatecommand category and selectImport Certificate. - UnderImport Certificateon the command card, in theSourcebox, selectUSBorSD Card.
- In theFileNamebox, type the file name of the certificate or or create a binding to a string which contains the file name of the certificate.
Provide Feedback