- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Add an event command to open Logix Designer
Add an event command to open
Logix Designer
. The command opens Logix Designer
from the Emulator or a View 5000 Client
of a project configured for a View 5000 Server
HMI device. PanelView
5000 HMI devices do not support opening Logix Designer
. - State Enter. Occurs when a graphic element, Add-On Graphic, screen, popup, or the System Banner transitions into the selected state through an animation.Prerequisites
- Create an event to trigger the command:
- Touch press.Occurs when touching the item on the screen that is configured with the event.
- Touch release.Occurs when releasing the item on the screen that is configured with the event.
- Key press.Occurs when
- Key release.Occurs when releasing the specified key.
To add an event command to open
Logix Designer
- Expand the
- Select the graphic element configured with the touch or key event.
- In thePropertiespane on theEventstab, selectAdd Command.
Windowscategory and selectOpen Logix Designer. - Specify the .ACD file and the location in the file to open:
- In theProjectFilebox, browse to select the file to open.
- In theProgramNamebox, enter the program to open.
- In theRoutineNamebox, enter the routine to open.
- In theRungNumberbox, enter the rung number to open.
Provide Feedback