Add a column to the Automatic Diagnostics or Automatic Diagnostics History tables

Add a column to the Automatic Diagnostics or Automatic Diagnostics History tables

New columns in tables appear on the right side of the table with sample data inserted into each column. Sample data is a representative of the length of data in a column. Use sample data to determine the column width.
To add a column to the Automatic Diagnostics or Automatic Diagnostics History tables
  1. On the screen, select the
    Automatic Diagnostics
    or
    Automatic Diagnostics History
    table.
  2. In the
    Properties
    window, select the
    Columns
    tab.
  3. Select
    Add Column
    .
  4. Select the data to display in the column. The selected column appears in the new card heading. Change the width of a column to display the data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.