Change the order of columns in Automatic Diagnostics or Automatic Diagnostics History table

Change the order of columns in Automatic Diagnostics or Automatic Diagnostics History table

The columns of the automatic diagnostics tables on the predefined
Automatic Diagnostics
and
Automatic Diagnostics History
screens appear in a default order. The screen is located in the
Predefined Screens
folder of the
Project Explorer
.
To change the order of columns in a table
  1. On the screen, select the
    Automatic Diagnostics
    or
    Automatic Diagnostics History
    table.
  2. In the
    Properties
    window, select the
    Columns
    tab.
  3. Point to the column card heading and select
    Move column up
    Card Up Arrow in Designer or
    Move column down
    Card Down Arrow in Designer to move the column higher (to the left) or lower (to the right) in the table. Changes made to the order of columns are depicted in the table on the screen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.