Change the marker of a trace

Change the marker of a trace

Change the marker that depicts data samples on a trace. Markers have different shapes. Each trace can use a different marker to depict data samples. A trace does not have to have a marker.
To change the marker of data on trace
  1. Select the trend chart on the screen.
  2. In the
    Properties
    window, select the
    Traces
    tab.
  3. Expand the
    Trace
    card and the
    Appearance
    category.
  4. After the
    Marker
    box, select the arrow to select a marker:
    • None
    • ViewRTLineMarker6 Star
    • ViewRTLineMarker4 Cross
    • ViewRTLineMarker8 Circle
    • ViewRTLineMarker2 Square
    • ViewRTLineMarker4 Triangle
    • ViewRTLineMarker3 Filled Circle
    • ViewRTLineMarker7 Filled Square
    • ViewRTLineMarker1 Filled Triangle
      The selected marker appears on the trace in the trend chart on the HMI device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.