- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Hide the axes on a trend chart
Hide the axes to customize the appearance of a trend chart. Hiding the axes hides both the y-axis and the time axis, including all labels and tick marks.
To hide the axes on a trend chart
- Select the trend chart on the screen.
- In thePropertieswindow, select thePropertiestab.
- Expand theAppearancecategory.
- Clear theShowAxesbox to hide the axes, tick marks, and labels. Select the box to show these items on the trend chart.
Provide Feedback