- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
What is a trend chart?
A trend chart is a graph of data from the system. For example, a trend chart can monitor tank pressure and tank temperature over the course of an hour.
Use a trend chart to:
- Monitor processes in a manufacturing system
- Display data from a tag, user-defined property, or the property of a graphic element
- Display up to eight traces that plot data over time to graphically present data
- View, pan, and pause data on the HMI device
Provide Feedback