Download and upload a project

Download and upload a project

View Designer
provides a
Download Runtime Application
wizard to build the runtime application from your project and transfer it to the HMI device.
View Designer
verifies a project automatically when you download a project to the HMI device. Invalid tags or expressions are listed in the
Errors
window.
View Designer
also provides an
Upload Runtime Application
wizard to transfer a runtime application from an HMI device to a computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.