- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Change the sample rate of a data log
Change the sample rate of a data log to change how often the data log collects tag values, in milliseconds, on the HMI device. For example, to collect data every 30 seconds, specify 30,000 milliseconds as the sample rate. The default sample rate is 1,000 milliseconds or every second. Valid sample rates range from 500 milliseconds to 60,000 milliseconds.
To change the sample rate of a data log
- In theProject Explorer, expand theData Logsfolder and double-click the data log. The data log opens in theData Logtab.TIP:Right-clicking the data log in theData Logsfolder and clickingOpenopens the data log.
- In the box afterSample Rateat the top of the data log, select how often the data log collects data. For example, select500ms to have the data log collect data every half second.TIP:Tips:
- Changing the sample rate causes previously collected data to no longer appear in the data log when the project downloads again.
- If there is no change to the sample rate, log duration, or number of tags in the data log, previously collected data in the data log remains unchanged when re-downloading the project to the HMI device.
- TheSample Ratebox has a red outline if it does not contain a valid entry.
- The data log contains tag values with the specified sample rate from all controllers.
Provide Feedback