Redo an action

Redo an action

Redo the most recent edit to a screen, popup, or the definition of an Add-On Graphic.
View Designer
tracks edits made to an open screen, popup, or definition of an Add-On Graphic. Each screen, popup, and Add-On Graphic definition has its redo history.
Closing a screen, popup, or Add-On Graphic definition clears redo actions to perform on that screen, popup, or Add-On Graphic definition. When re-opening the screen, popup, or Add-On Graphic definition, the previous actions are not available to redo.
To redo an action
  • On the
    Standard
    toolbar, select
    Redo
    Icon: View Designer Redo Icon. The last undone action is redone.
    TIP:
    Tips:
    • Place the cursor over theIcon: View Designer Redo Icon button to show the action to be redone.
    • Alternative methods for redoing an action include:
      • Press
        CTRL+Y
        .
      • Select
        Edit > Redo
        .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal