- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Events and Add-On Graphics
Add events to an instance of an Add-On Graphic on a screen or to a graphic element in the definition of an Add-On Graphic. As with groups, events for the content in the definition of an Add-On Graphic trigger in a specific order.
Adding events to an Add-On Graphic in the
Toolbox
is not allowed. Selecting an Add-On Graphic in the Toolbox
does not show the the Events
tab in the Properties
window. Events created for an instance of an Add-On Graphic take precedence over events created for a graphic element within the definition of the Add-On Graphic. For example, if the same event type exists in both the definition of an Add-On Graphic and an instance of that Add-On Graphic, the event for the instance of the Add-On Graphic is performed on the HMI device.
Provide Feedback