Select a default language for HMI device

Select a default language for HMI device

Select a default language for HMI devices to use for a download or restart.
To select a default language for HMI device
  1. On the
    Project Properties
    dialog box, select the
    Language
    tab.
  2. Select the
    Default language for HMI device startup
    list, select a language, and select
    OK
    .
    TIP:
    If the
    Default language for HMI device startup
    list is disabled, import languages to enable the list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.