Undo an action

Undo an action

Undo the most recent edits made to a screen, popup, or the definition of an Add-On Graphic.
View Designer
tracks edits made to an open screen, popup, or definition of an Add-On Graphic. Each screen, popup, and Add-On Graphic definition has its own undo history. Changes made to the definition of an Add-On Graphic after deleting an instance of the Add-On Graphic apply to the instance when undoing the deletion of the instance.
Closing a screen, popup, or Add-On Graphic definition clears the undo actions to perform on that screen, popup, or Add-On Graphic definition. When re-opening the screen, popup, or Add-On Graphic definition, the previous actions are not available to undo.
TIP:
Tips:
  • Undo is not available for some actions, such as finding and replacing text in a project or ungrouping grouped graphic elements.
  • Undoing changes made to
    Project Explorer
    (for example, deleting a screen),
    Project Properties
    (for example, deleting a controller), or
    Security Administration
    (for example, deleting a user) is not supported.
To undo an action:
  • On the
    Standard
    toolbar, select
    Undo
    Icon: View Designer Undo Icon. The most recent action is undone.
    TIP:
    Tips:
    • Place the cursor over the Icon: View Designer Undo Icon button to show the action to be undone.
    • Alternative methods for undoing an action include:
      • Press
        Ctrl+Z.
      • Select
        Edit > Undo
        .
      • Changes to the definition of an Add-On Graphic appear in a previously deleted instance of the Add-On Graphic when deleting an instance, changing the definition, and then undeleting the instance. For example, any changes to the content, an alias, a binding, or a value appear in the undeleted instance of the Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal