- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Remove a controller reference
Removing a controller reference disconnects the or .
View Designer
project from the Logix Designer
project file (.acd). Tags and data types for the referenced controller no longer appear in the Tag Browser
Data Type Browser
To remove a controller reference
- On theProject Propertiesdialog box, select theReferencestab.
- To the right of the controller reference, selectRemove controller reference. The reference no longer appears.TIP:Tips:
- Removing a controller reference adjusts the placement of any subsequent reference cards. After saving controller references, reference cards appear in order by controller reference number that appears in theController[#] Reference Namebox.
- In theControllerspopup on the HMI device, any unused controller reference has a tab namedNot configured.
- SelectApplyto save changes and remain on theProject Propertiesdialog box, or selectOKto save changes and close theProject Propertiesdialog box.
Provide Feedback