- Studio 5000 View Designer Help
- Add a graphic element to a project
- Graphic elements library
- Reuse content
- Add-On Graphics
- Change a property
- Bind properties
- Display Automatic Diagnostics
- Use the runtime application
Copy a shortcut
Copy a shortcut to reuse it within a project.
To copy a shortcut
- In theProject Explorer, expand theNavigation Menufolder.
- Right-click the shortcut and selectCopy.TIP:To select multiple shortcuts, holdCtrland select the items.
- Right-click the location in the targetNavigation Menufolder and selectPaste.
- If the target folder contains a shortcut with the same name, selectKeep Bothto keep both shortcuts. The name of the new shortcut is appended with a number to distinguish it from the original.TIP:Tips:
- Copying an item from a folder in theProject Explorerand then pasting it in the same folder in the same project creates a copy of the item. The name of the pasted item is appended with a number that increments with each copy.
- Copy and paste shortcuts in theNavigation Menufolder only.
Provide Feedback