Open a shortcut

Open a shortcut

Open a shortcut to:
  • View its contents.
  • Change the contents of the screen that defines the shortcut.
  • Change the values of any user-defined screen properties that are passed to the defining screen of the shortcut.
Changing the contents of a shortcut is not allowed.
To open a shortcut
  1. In the
    Project Explorer
    , expand the
    Navigation Menu
    folder.
  2. Double-click the shortcut. The shortcut opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.