N - Z

N - Z

relative path
A path that specifies the location of a directory relative to another directory.
runtime
The period of time during which the HMI project file is running on the HMI device from startup to shutdown.
screen parameter
An aliased property that is used to pass tag values to a screen at runtime. It is one of the many methods used to reuse content and simplify screen creation.
system tag
A predefined tag that provides information about your system, such as the current logged-in user and the current time and date.
.VPD
The file extension for project files created using the
Studio 5000
View Designer
software.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal